PCA9420 (How to change SW2 default 1.8V output to 3.3V output)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9420 (How to change SW2 default 1.8V output to 3.3V output)

Jump to solution
962 Views
Selamu
Contributor I

Hi community,

We use a PCA9420 PMIC on our design and would like to change BUCK2 (SW2, system buck regulator) default 1.8V output to 3.3V. I checked the datasheet and it shows that, on page 15, the SW2 output voltage can be programmed via I2C register from 1.5V to 2.1V, or from 2.7V to 3.3V in both at 25mV/step, but the maximum voltage which is available to select on all mode settings is 2.1V.

anybody has an idea on how it will be changed to 3.3V?

Regards

0 Kudos
Reply
1 Solution
952 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Selamu,

In order to set SW2 output voltage in the range of 2.7V to 3.3V, the SW2_OUT_1_OFFSET bit needs to be set to 1:

Table 54.JPG

Then SW2 Output Voltage = SW2_OUT_1_LSB[4:0] + 1.2V, so if you set SW2_OUT_1_LSB[4:0] = 0b11001-0b11111 = 2.1V, then SW2 = 2.1V + 1.2V = 3.3V

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
1 Reply
953 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Selamu,

In order to set SW2 output voltage in the range of 2.7V to 3.3V, the SW2_OUT_1_OFFSET bit needs to be set to 1:

Table 54.JPG

Then SW2 Output Voltage = SW2_OUT_1_LSB[4:0] + 1.2V, so if you set SW2_OUT_1_LSB[4:0] = 0b11001-0b11111 = 2.1V, then SW2 = 2.1V + 1.2V = 3.3V

Best regards,

Tomas

0 Kudos
Reply