KITPF09FRDMPGM – Wrong Board Included?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KITPF09FRDMPGM – Wrong Board Included?

875 Views
d_j
Contributor V

I ordered a KITPF09FRDMPGM. The delivery included the KITPF09FRDMPGM and a separate FRDM-KL25Z board.

However, I don't think the two boards are compatible, or at least I don't see how they are supposed to be connected. For example, the J21 header on the FRDM-KL25Z is mechanically in the way.

In addition, the pin headers required to plug the KITPF09FRDMPGM into the FRDM-KL25Z are missing.

Could somone please confirm whether the correct board was included with the kit? Shouldn't it look similar to the board supplied with the KITPF7100FRDMPGM?

Labels (1)
0 Kudos
Reply
12 Replies

490 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello @d_j @florian_arndt 

I don’t think a video is necessary at this point. First, please note that connector J21 does not interfere with the PF09 board.

ErikaC_2-1792002102847.png

ErikaC_3-1792002114951.png

 

Second, please find attached the firmware for the PF09 board. I tested it on my side, and it is working correctly.

ErikaC_1-1792002043210.png

Hope this helps!

Best regards,
Erika

 

0 Kudos
Reply

350 Views
d_j
Contributor V

Hi Erika,

thank you for your answer!

Here are my steps:

1. I've checked J21 and can confirm, there ist no contact to the upper board

2. I've downloaded your firmware file

2. I've pressed reset button and connected USB to the OpenSDA connector

3. I've copied the firmware file in the explorer drive BOOTLOADER

4. I've connected USB to KL25Z USB connector

Unfortunately, the status in the NXP GUI still keeps switching between "NOT CONNECTED" and "DISCONNECTED," and the Start button remains grayed out.

0 Kudos
Reply

493 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello @d_j @florian_arndt 

Let me check and see if I can send you a video!
0 Kudos
Reply

495 Views
karina_valencia
NXP Apps Support
NXP Apps Support

@ErikaC can you continue with the support?

0 Kudos
Reply

814 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

The board included with the KITPF09FRDMPGM is the correct board. The KITPF09FRDMPGM and the FRDM-KL25Z are supplied as separate boards and are compatible when assembled as intended.

The required pin headers are not included pre-installed and must be purchased separately and soldered onto the boards. Once the appropriate headers are installed, the boards can be connected correctly.

I have tested the KITPF09FRDMPGM board without any problems, so the board itself is correct and functional.

Hope this helps!

0 Kudos
Reply

801 Views
d_j
Contributor V

I have now soldered on the headers. However, nothing happens when I try to connect the kit using the NXP_GUI. I also found an old kit for the PF8100 with an older FRDM-KL25Z; that one is detected. What could be wrong?

0 Kudos
Reply

776 Views
d_j
Contributor V

Perhaps I bricked the firmware. Can you tell me if this the correct firmware: OpenSDA/PEMicro/2016-02-08/MSD-DEBUG-FRDM-KL25Z_Pemicro_v118.SDA at master · savoca/OpenSDA · GitHub

...or can you give me the link to the correct firmware?

0 Kudos
Reply

601 Views
florian_arndt
Senior Contributor I

Hello @ErikaC,

as I am a colleague from d_j:
Can you please check his question and provide us with information, which firmware is needed for this board? We both can not establish the connection as the "start" button is inactive. We both use Win11, not Win10 as suggested by the documentation.

Thank you in advance.

Best regards,
Florian

0 Kudos
Reply

497 Views
florian_arndt
Senior Contributor I

Hello @ErikaC,

can you please give us any hint or ask other colleagues?

Thank you in advance.

Best regards,
Florian

0 Kudos
Reply

809 Views
d_j
Contributor V

I’m still surprised that it’s supposed to fit. The outline is different, and connector J21 interferes with the board. Should I desolder it?

KITPF09FRDMPGM.png

Shouldn't the controller board look more like this?

KITPF7100FRDMPGM-ASSEMBLY.png

  

0 Kudos
Reply

490 Views
ErikaC
NXP TechSupport
NXP TechSupport

Please solder female headers onto the KL25 side.

0 Kudos
Reply

804 Views
d_j
Contributor V

Okay, I’ve thought about it again. J21 is probably just a jumper and won't interfere with the top board if the pin headers are installed. I'll give it a try.

0 Kudos
Reply