Hello,
The board included with the KITPF09FRDMPGM is the correct board. The KITPF09FRDMPGM and the FRDM-KL25Z are supplied as separate boards and are compatible when assembled as intended.
The required pin headers are not included pre-installed and must be purchased separately and soldered onto the boards. Once the appropriate headers are installed, the boards can be connected correctly.
I have tested the KITPF09FRDMPGM board without any problems, so the board itself is correct and functional.
Hope this helps!