How does the PCA9450 behave after its output is shorted?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How does the PCA9450 behave after its output is shorted?

Jump to solution
1,363 Views
tomo
Contributor II

Hi all,

How does the PCA9450 behave after the output is shorted?
I'm assuming that after a short occurs, all outputs are stopped once, but after that, does the PCA9450 try to restart the outputs like in HICCUP mode? Or does it keep stopping output?

Best regards,

tomo

Tags (1)
0 Kudos
Reply
1 Solution
1,354 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Miyazaki-san,

If the PMIC is in RUN/STBY mode, this behavior of all outputs are stopped once happens at the VRFLTx is unmasked, and after tFLT_POK_MSK, the regulators are trying to restart like HICCUP. But if masked, only the fault regulator stopped. Once short event removed, the output is normal, but there will be an interrupt and a fault status register assert.

BR, Tomas

View solution in original post

0 Kudos
Reply
2 Replies
1,355 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Miyazaki-san,

If the PMIC is in RUN/STBY mode, this behavior of all outputs are stopped once happens at the VRFLTx is unmasked, and after tFLT_POK_MSK, the regulators are trying to restart like HICCUP. But if masked, only the fault regulator stopped. Once short event removed, the output is normal, but there will be an interrupt and a fault status register assert.

BR, Tomas

0 Kudos
Reply
1,335 Views
tomo
Contributor II

Thank you for your reply.

I understand the content of your reply.
thank you very much.

Best regards,
tomo

0 Kudos
Reply