FS8530 with FlexGUI: OTP programming error Boot Enable (BE) failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FS8530 with FlexGUI: OTP programming error Boot Enable (BE) failed

跳至解决方案
3,895 次查看
BL_
Contributor III

Hi,

We want to burning/programming the OTP for FS8530 PMIC using FlexGUI.

In OTP emulation mode, everything works fine. I could send the generated script (from Excel file) to the FS8530 PMIC and the device behaves as expected.

Then I proceeded the OTP programming as follow:

  • Restart the PMIC device by turning Vbat Off and On again via SW1-switch
  • In "OTP_prog" tab, I browsed to the generated script and clicked on "program" button
  • As the pop-up windows appeared, I turned on the DBG_pin by closing SW3-switch

And now came the error: "Boot Enable (BE) failed".

After this process, when I start the device, it consumes a lot of current (~400mA) and the outputs of the regulators are not switched on.

I don't know what went wrong? and How to solve the error ?

Here is a screen shot from FLexGui.

BL__0-1647010590756.pngBL__0-1647010590756.png

Thanks,

BL

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
3,883 次查看
BL_
Contributor III

as it turned out, the OTP programming of A1 version had been adready done and can't be done again.

https://community.nxp.com/t5/Power-Management/FS8530-Is-OTP-Programming-Burning-possible-for-variant...

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
3,884 次查看
BL_
Contributor III

as it turned out, the OTP programming of A1 version had been adready done and can't be done again.

https://community.nxp.com/t5/Power-Management/FS8530-Is-OTP-Programming-Burning-possible-for-variant...

 

0 项奖励
回复