FS8530 with FlexGUI: OTP programming error Boot Enable (BE) failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS8530 with FlexGUI: OTP programming error Boot Enable (BE) failed

ソリューションへジャンプ
4,004件の閲覧回数
BL_
Contributor III

Hi,

We want to burning/programming the OTP for FS8530 PMIC using FlexGUI.

In OTP emulation mode, everything works fine. I could send the generated script (from Excel file) to the FS8530 PMIC and the device behaves as expected.

Then I proceeded the OTP programming as follow:

  • Restart the PMIC device by turning Vbat Off and On again via SW1-switch
  • In "OTP_prog" tab, I browsed to the generated script and clicked on "program" button
  • As the pop-up windows appeared, I turned on the DBG_pin by closing SW3-switch

And now came the error: "Boot Enable (BE) failed".

After this process, when I start the device, it consumes a lot of current (~400mA) and the outputs of the regulators are not switched on.

I don't know what went wrong? and How to solve the error ?

Here is a screen shot from FLexGui.

BL__0-1647010590756.png

Thanks,

BL

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,992件の閲覧回数
BL_
Contributor III

as it turned out, the OTP programming of A1 version had been adready done and can't be done again.

https://community.nxp.com/t5/Power-Management/FS8530-Is-OTP-Programming-Burning-possible-for-variant...

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,993件の閲覧回数
BL_
Contributor III

as it turned out, the OTP programming of A1 version had been adready done and can't be done again.

https://community.nxp.com/t5/Power-Management/FS8530-Is-OTP-Programming-Burning-possible-for-variant...

 

0 件の賞賛
返信