FS8530 FlexGUI: Does the GUI work with Adoptium Prebuilt OpenJDK Binary?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS8530 FlexGUI: Does the GUI work with Adoptium Prebuilt OpenJDK Binary?

2,681件の閲覧回数
BL_
Contributor III

Hi,

Since we currently encounter a trouble with the Java license, we would like to know whether the FS8530 FlexGUI is also working with Prebuilt OpenSDK (Eclipse Temurin) from Adoptium ?

 

Thanks.

BL

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,677件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Bien,

Adoptium OpenJDK build version 8 (LTS) can also be used for the FS85 GUI, see:

https://adoptium.net/?variant=openjdk8&jvmVariant=hotspot

It is important to choose an OpenJDK build that also contains JavaFX modules, such as Azul, Belsoft Liberica, Amazon Correto or Eclipse Temurin.

Best regards,

Tomas

0 件の賞賛
返信

2,672件の閲覧回数
BL_
Contributor III

Hi Tomas,

thanks for the quick response.

I'm using the "jre-8.0.312.7-hotspot" from Eclipse Temurin. However when running the "flexgui-app-spm.bat" file, it does not do anything.

I had this problem before and solved it by setting "JAVA_HOME" variable to correct path. As described here: https://community.nxp.com/t5/Power-Management/FlexGUI-for-FS85-FS84-Evaluation-Tools-quot-bat-quot-f...

Now even though I have set the "JAVA_HOME" variable to "C:\Program Files\Eclipse Adoptium\jre-8.0.312.7-hotspot", "flexgui-app-spm.bat" file still does nothing.

Do you have an idea what could went wrong?

Thanks,

BL

0 件の賞賛
返信