Hi Team,
We are using FS2600D. This do not have Tracker 2 and FS1B as seen in datasheet.
So regarding pin 5 (TRK2), pin12 (FS1B) and pin38 (n.c):
1) Does these pins have any internal connection or is it physically no connection.
2) Should I leave these floating. Or put a capacitor for immunity on these pins.
Basically we don't want to risk EMI noises on these unused pins affecting the IC functionality.
Looking forward for answers and recommendations.
Solved! Go to Solution.
Hello MVCJ,
I hope all is great with you. Thank you for using the NXP communities.
Please review the recommended connection in case such pins are not used.
TRK2 - Open - TRK2 to be configured OFF for power up sequence TRK2_SLOT_OTP[2:0] = 111
FS1B - Open - 2 MΩ internal pulldown
NC – Not applicable
You may find further information at Table 4 from the datasheet.
Those pins (TRK2 and FSIB) have internal connections. You can find detailed information at the application note AN12995 (NXP FS26 Hardware Guidelines) from your secure files.
I hope this information helps.
Regards,
David
Hello MVCJ,
I hope all is great with you. Thank you for using the NXP communities.
Please review the recommended connection in case such pins are not used.
TRK2 - Open - TRK2 to be configured OFF for power up sequence TRK2_SLOT_OTP[2:0] = 111
FS1B - Open - 2 MΩ internal pulldown
NC – Not applicable
You may find further information at Table 4 from the datasheet.
Those pins (TRK2 and FSIB) have internal connections. You can find detailed information at the application note AN12995 (NXP FS26 Hardware Guidelines) from your secure files.
I hope this information helps.
Regards,
David