FS26 unconnected pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS26 unconnected pins

ソリューションへジャンプ
2,058件の閲覧回数
MVCJ
Contributor I

Hi Team,

We are using FS2600D. This do not have Tracker 2 and FS1B as seen in datasheet.

So regarding pin 5 (TRK2), pin12 (FS1B) and pin38 (n.c):

1) Does these pins have any internal connection or is it physically no connection.

2) Should I leave these floating. Or put a capacitor for immunity on these pins.

Basically we don't want to risk EMI noises on these unused pins affecting the IC functionality.

Looking forward for answers and recommendations.

0 件の賞賛
返信
1 解決策
2,050件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello MVCJ,

I hope all is great with you. Thank you for using the NXP communities.

Please review the recommended connection in case such pins are not used.

TRK2 - Open - TRK2 to be configured OFF for power up sequence TRK2_SLOT_OTP[2:0] = 111

FS1B - Open - 2 MΩ internal pulldown

NC – Not applicable

You may find further information at Table 4 from the datasheet.

Those pins (TRK2 and FSIB) have internal connections. You can find detailed information at the application note AN12995 (NXP FS26 Hardware Guidelines) from your secure files.

I hope this information helps.

Regards,

David

元の投稿で解決策を見る

1 返信
2,051件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello MVCJ,

I hope all is great with you. Thank you for using the NXP communities.

Please review the recommended connection in case such pins are not used.

TRK2 - Open - TRK2 to be configured OFF for power up sequence TRK2_SLOT_OTP[2:0] = 111

FS1B - Open - 2 MΩ internal pulldown

NC – Not applicable

You may find further information at Table 4 from the datasheet.

Those pins (TRK2 and FSIB) have internal connections. You can find detailed information at the application note AN12995 (NXP FS26 Hardware Guidelines) from your secure files.

I hope this information helps.

Regards,

David