Security Engine inside P5040

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Security Engine inside P5040

Jump to solution
1,547 Views
weizhao
Contributor I

Hi,

We're using P5040 QorIQ Integrated Multicore Communication Processor in our products.  According to P5040 manual, there is a security engine inside P5040, and we'd like to use i as Random Number Generator.  Is there any application note for the security engine using ?

Thanks,

Wei

0 Kudos
Reply
1 Solution
1,383 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

There is separate P5040 Security (SEC) Reference Manual on the P5040 web page

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-powe...

There are application notes for the SEC 2.0 and SEC 3.x but it is not so useful because the P5040 has SEC rev. 4.2. You can search for the security training courses on the NXP site. For example see “Introduction to Security Acceleration in QorIQ Processors”

https://community.nxp.com/servlet/JiveServlet/downloadBody/331881-102-1-267794/DES-N1856%20Security%...

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,384 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

There is separate P5040 Security (SEC) Reference Manual on the P5040 web page

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-powe...

There are application notes for the SEC 2.0 and SEC 3.x but it is not so useful because the P5040 has SEC rev. 4.2. You can search for the security training courses on the NXP site. For example see “Introduction to Security Acceleration in QorIQ Processors”

https://community.nxp.com/servlet/JiveServlet/downloadBody/331881-102-1-267794/DES-N1856%20Security%...

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply