P5040DS-PB demo board boot flash access using JTAG tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P5040DS-PB demo board boot flash access using JTAG tool

1,269 Views
rammurmu
Contributor III

Hi,

I am using P5040DS-PB demo board. I need to access the boot flash (NOR flash 128MB) using the JTAG tool. What are the registers that need to be configured for proper board initialization , so that using the JTAG tool I can access the boot flash(NOR flash). I have verified the following register configuration - CCSRBAR, TLB, LAW, CS, Flash Part No. and Sector size but no luck.

Please suggest.

Regards

Ram

Labels (1)
4 Replies

1,026 Views
ufedor
NXP Employee
NXP Employee

Which "JTAG tool" is in question?

The CodeWarrior Flash Programmer could be used to program the P5040DS NOR Flash using attached initialization file.

0 Kudos
Reply

1,026 Views
rammurmu
Contributor III

Thanks ufedor.

I am using Lauterbach Trace32 JTAG tool.

0 Kudos
Reply

1,026 Views
ufedor
NXP Employee
NXP Employee

It is reasonable to address the question to the Lauterbach Technical Support.

1,026 Views
rammurmu
Contributor III

Thank you ufedor.

0 Kudos
Reply