How can I get "fsl_fman_ucode_p4080_r2.0_106_2_15.bin" for P4080 revision 2.0 using QorIQ Linux SDK 2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I get "fsl_fman_ucode_p4080_r2.0_106_2_15.bin" for P4080 revision 2.0 using QorIQ Linux SDK 2.0

714 Views
paramahansapolo
Contributor I

Hello,

I'm doing the bring up on a customized board that uses P4080 revision 2.0
Also, I'm using QorIQ Linux SDK v2.0

According to the docs (QorIQ_SDK_2.0.pdf); I should use the FMAN microcode binary "fsl_fman_ucode_p4080_r2.0_106_2_15.bin".
But, it doesn't seems to be built when compiling the SDK.
I would appreciate if anybody could tell me: How do I build it?  Or how can I get that microcode binary?
Many thanks in advance,

-Paramahansa

Labels (1)
0 Kudos
Reply
1 Reply

469 Views
ufedor
NXP Employee
NXP Employee

The FMan microcode binary image is not built during the SDK compilation and provided "as is".

Please note that according to the SDK v2.0 Documentation only P4080 Rev.3.0 is supported - refer to:
https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-21A68B1F-4CD4-4959-9175-4...
This is why the "fsl_fman_ucode_p4080_r3.0_106_2_18.bin" is provided in the "QorIQ Linux SDK v2.0 PPCE500MC IMAGE.iso".

The "fsl_fman_ucode_p4080_r2.0_106_2_15.bin" is included into the SDK v1.8 and provided on the "QorIQ-SDK-v1.8-PPCE500MC-IMAGE-20150619-yocto.iso" available at:
https://freescaleesd.flexnetoperations.com/337170/17/8922017/QorIQ-SDK-v1.8-PPCE500MC-IMAGE-20150619...

0 Kudos
Reply