P5040DS-PB demo board boot flash access using JTAG tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P5040DS-PB demo board boot flash access using JTAG tool

1,270 次查看
rammurmu
Contributor III

Hi,

I am using P5040DS-PB demo board. I need to access the boot flash (NOR flash 128MB) using the JTAG tool. What are the registers that need to be configured for proper board initialization , so that using the JTAG tool I can access the boot flash(NOR flash). I have verified the following register configuration - CCSRBAR, TLB, LAW, CS, Flash Part No. and Sector size but no luck.

Please suggest.

Regards

Ram

标签 (1)
4 回复数

1,027 次查看
ufedor
NXP Employee
NXP Employee

Which "JTAG tool" is in question?

The CodeWarrior Flash Programmer could be used to program the P5040DS NOR Flash using attached initialization file.

0 项奖励
回复

1,027 次查看
rammurmu
Contributor III

Thanks ufedor.

I am using Lauterbach Trace32 JTAG tool.

0 项奖励
回复

1,027 次查看
ufedor
NXP Employee
NXP Employee

It is reasonable to address the question to the Lauterbach Technical Support.

1,027 次查看
rammurmu
Contributor III

Thank you ufedor.

0 项奖励
回复