P2020 Processor PWR Dissipation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2020 Processor PWR Dissipation

2,533件の閲覧回数
nicholas_harvey
Contributor I

Does anyone know how to calculate estimated power dissipation of a P2020NXE2MHC processor running at an internal core speed of 400MHZ? The DDR3 interface runs internally at 800MZ and externally at 400MHZ. 

0 件の賞賛
返信
3 返答(返信)

2,477件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the AN4261 - P2020 QorIQ Integrated Processor Design Checklist, Table 11. Processor Clocking Range where it is stated that minimum Core clock frequency is 533 MHz.

What is CCB/Platform frequency?

0 件の賞賛
返信

2,477件の閲覧回数
nicholas_harvey
Contributor I

The CCB/Platform frequency is 600MHz.

0 件の賞賛
返信

2,477件の閲覧回数
ufedor
NXP Employee
NXP Employee

> The CCB/Platform frequency is 600MHz.

What is Core clock frequency?

0 件の賞賛
返信