P2020 Processor PWR Dissipation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 Processor PWR Dissipation

2,578 Views
nicholas_harvey
Contributor I

Does anyone know how to calculate estimated power dissipation of a P2020NXE2MHC processor running at an internal core speed of 400MHZ? The DDR3 interface runs internally at 800MZ and externally at 400MHZ. 

0 Kudos
Reply
3 Replies

2,522 Views
ufedor
NXP Employee
NXP Employee

Please refer to the AN4261 - P2020 QorIQ Integrated Processor Design Checklist, Table 11. Processor Clocking Range where it is stated that minimum Core clock frequency is 533 MHz.

What is CCB/Platform frequency?

0 Kudos
Reply

2,522 Views
nicholas_harvey
Contributor I

The CCB/Platform frequency is 600MHz.

0 Kudos
Reply

2,522 Views
ufedor
NXP Employee
NXP Employee

> The CCB/Platform frequency is 600MHz.

What is Core clock frequency?

0 Kudos
Reply