P2020 64B network packet forwarding speed is much?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 64B network packet forwarding speed is much?

1,111 Views
fanghua
Contributor II

I want to know how much P2020 64B network packet forwarding speed is ? 

0 Kudos
Reply
1 Reply

951 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello fang hua,

In SDK 1.9 testing, we got throughput about 410.59 Mbps on one P2020RDB target board in the scenario IPv4 FWD SMP 2 cores two flows at 64 Bytes FrameSize  with CPU/DDR/DDB clock at 1200/400/600.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply