P2020 64B network packet forwarding speed is much?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P2020 64B network packet forwarding speed is much?

1,109 次查看
fanghua
Contributor II

I want to know how much P2020 64B network packet forwarding speed is ? 

0 项奖励
回复
1 回复

949 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello fang hua,

In SDK 1.9 testing, we got throughput about 410.59 Mbps on one P2020RDB target board in the scenario IPv4 FWD SMP 2 cores two flows at 64 Bytes FrameSize  with CPU/DDR/DDB clock at 1200/400/600.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复