P1020RDB PCIE interface issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

P1020RDB PCIE interface issue

跳至解决方案
1,340 次查看
yinux
Contributor III

hello all ,

     env: vxworks, p1020rdb.

     the target.ref show as follows:

      PCI-E-HOST:0       | on-chip    |                     | UNSUPPORTED

      PCI-E-HOST:1       | on-chip    | m85xxPci.c          | SUPPORTED

     0x9000_0000 | 64MB  | 0x93FF_FFFF | PCIe-2 Memory

     0x9400_0000 | 64MB  | 0x97FF_FFFF | PCIe 2 Non-Prefetchable Memory

     0x9800_0000 | 64MB  | 0x9BFF_FFFF | PCIe 2 I/O Memory

      2 questions as follows:

     1) if i want to use the 2 pcie interface, the host controller of PCIE-HOST0  is the same as m85xxPci.c   ?

         i just need to modify the hwconf.c, syslib.c,and  p1020rdb.h ?

     2) in the p1020RM.pdf,

         pastedImage_0.png

          the  base address of pcie2  canbe set as 0x9000_00000?

          the base  address of pcie1 canbe set as 0xa000_00000?

          i am confused, thanks for all reply.

标签 (1)
0 项奖励
回复
1 解答
1,078 次查看
yinux
Contributor III

i understand the meaning. no issue.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,079 次查看
yinux
Contributor III

i understand the meaning. no issue.

0 项奖励
回复