P1020RDB PCIE interface issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1020RDB PCIE interface issue

Jump to solution
1,341 Views
yinux
Contributor III

hello all ,

     env: vxworks, p1020rdb.

     the target.ref show as follows:

      PCI-E-HOST:0       | on-chip    |                     | UNSUPPORTED

      PCI-E-HOST:1       | on-chip    | m85xxPci.c          | SUPPORTED

     0x9000_0000 | 64MB  | 0x93FF_FFFF | PCIe-2 Memory

     0x9400_0000 | 64MB  | 0x97FF_FFFF | PCIe 2 Non-Prefetchable Memory

     0x9800_0000 | 64MB  | 0x9BFF_FFFF | PCIe 2 I/O Memory

      2 questions as follows:

     1) if i want to use the 2 pcie interface, the host controller of PCIE-HOST0  is the same as m85xxPci.c   ?

         i just need to modify the hwconf.c, syslib.c,and  p1020rdb.h ?

     2) in the p1020RM.pdf,

         pastedImage_0.png

          the  base address of pcie2  canbe set as 0x9000_00000?

          the base  address of pcie1 canbe set as 0xa000_00000?

          i am confused, thanks for all reply.

Labels (1)
0 Kudos
Reply
1 Solution
1,079 Views
yinux
Contributor III

i understand the meaning. no issue.

View solution in original post

0 Kudos
Reply
1 Reply
1,080 Views
yinux
Contributor III

i understand the meaning. no issue.

0 Kudos
Reply