P1011 maximum clock input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1011 maximum clock input

1,891 Views
danielminors
Contributor I

I cannot find any detail on the datasheet regarding the tolerance of the 100MHz maximum clock input for the P1011 processor. What is the maximum clock PPM that can be used when supplied with a 100MHz source?

0 Kudos
Reply
2 Replies

1,835 Views
yipingwang
NXP TechSupport
NXP TechSupport

The 100MHz SYSCLK supports spread spectrum on P1011
So essentially there is no ppm restriction on this clock.

0 Kudos
Reply

1,864 Views
yipingwang
NXP TechSupport
NXP TechSupport

Confirming with the AE team.

0 Kudos
Reply