P1010 reports "Data Cache Parity Error"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1010 reports "Data Cache Parity Error"

1,912 Views
qingshanli
Contributor I

CPU:P1010

OS: linux-3.8.13

Error information output from linux as below:

kernel-2: Machine check in kernel mode.

kernel-2: Caused by (from MCSR=10000000): Data Cache Parity Error

kernel-2:Oops: Machine check, sig: 7 [#1]

kernel-2:P1010

What's wrong with this CPU, and how to resolve this problem?

Labels (1)
0 Kudos
Reply
2 Replies

1,567 Views
alexander_yakov
NXP Employee
NXP Employee

Data cache parity error means data cache contents were checked for parity and resulting parity value is not equal to one stored in cache contents. This may mean:

1. Hardware failure - data corruption in data cache

2. Incorrect data cache parity information due to software error

For hardware failure case, please perform the following:

1. Please check how many (identical) boards you have and how many of them show such erratic behavior. If (for example) only one board fails out of (for example) 10, than this may mean a hardware failure of particular board.

2. Please check clocking configuration. Data cache may fail if the processor is running on speed higher than specified.

3. Please check power supply quality. The behavior may be a result of unstable operation due to power supply quality.

For second case - please check if the behavior is not specific to particular version of software you are running, for example if the problem appears on this version of the software and doe not appear on previous version.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,567 Views
qingshanli
Contributor I

Today we found another P1010 CPU report similar error:

kernel-2: Machine check in kernel mode.

kernel-2: Caused by (from MCSR=40000000): Instruction Cache Parity Error

kernel-2:Oops: Machine check, sig: 7 [#1]

kernel-2:P1010

0 Kudos
Reply