P1010 USB documentation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1010 USB documentation

ソリューションへジャンプ
1,548件の閲覧回数
smirnovalexey
Contributor I

Hello.

In the P1010RM in USB section we have a list of external signals.

For example Table 17-1 have an USB_DRVVBUS I/O signal. At the same time in P1010EC we have no such signal.

The closest alternative i can find is GPIO_0/IRQ_4/DRVVBUS/MDVAL pin D23.

Am I correct?

It is very confusing because of USB prefix absence..

Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,457件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

Yes, it is correct. Table 17-1 USB_DRVVBUS and DRVVBUS on pin D23 mean the same signal.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,458件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

Yes, it is correct. Table 17-1 USB_DRVVBUS and DRVVBUS on pin D23 mean the same signal.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信