P1010 USB documentation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

P1010 USB documentation

跳至解决方案
1,543 次查看
smirnovalexey
Contributor I

Hello.

In the P1010RM in USB section we have a list of external signals.

For example Table 17-1 have an USB_DRVVBUS I/O signal. At the same time in P1010EC we have no such signal.

The closest alternative i can find is GPIO_0/IRQ_4/DRVVBUS/MDVAL pin D23.

Am I correct?

It is very confusing because of USB prefix absence..

Thank you.

标签 (1)
0 项奖励
回复
1 解答
1,452 次查看
r8070z
NXP Employee
NXP Employee

Have a great day,

Yes, it is correct. Table 17-1 USB_DRVVBUS and DRVVBUS on pin D23 mean the same signal.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,453 次查看
r8070z
NXP Employee
NXP Employee

Have a great day,

Yes, it is correct. Table 17-1 USB_DRVVBUS and DRVVBUS on pin D23 mean the same signal.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复