Are there any environments or OS'es that allow WIndows or .NET applications to run on Power cores?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there any environments or OS'es that allow WIndows or .NET applications to run on Power cores?

Jump to solution
1,052 Views
Larry5335
Contributor IV

Customer wants to run .NET applications on a e6500 core. It is preferred to run a form of Linux on the e6500 core.

Are there any forms of Linux or add-ons that run on Power that can support .NET based applications?

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
853 Views
Larry5335
Contributor IV

Looks like the open source world is working on a solution:

http://www.mono-project.com/docs/about-mono/

.NET Framework Class Library - The Mono platform provides a comprehensive set of classes that provide a solid foundation to build applications on. These classes are compatible with Microsoft’s .Net Framework classes.

View solution in original post

0 Kudos
Reply
3 Replies
854 Views
Larry5335
Contributor IV

Looks like the open source world is working on a solution:

http://www.mono-project.com/docs/about-mono/

.NET Framework Class Library - The Mono platform provides a comprehensive set of classes that provide a solid foundation to build applications on. These classes are compatible with Microsoft’s .Net Framework classes.

0 Kudos
Reply
853 Views
ralftruebenbach
Contributor III

You could use a virtual i386 machine (e.g. qemu) and run wine or .NET for Linux in it. Don't know if this is really helpful but I think that's the closest you can get.

0 Kudos
Reply
853 Views
alexander_yakov
NXP Employee
NXP Employee

Sorry, we are unaware about any tools to run Windows or .NET applications to run on Power architecture.

I see .NET is available for several Linux distributions, still only x86/x64 architecture is supported.

.NET Downloads 


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply