Interrupt priority on the Linux P1020 - How to set it up?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interrupt priority on the Linux P1020 - How to set it up?

ソリューションへジャンプ
4,426件の閲覧回数
alfonsokame
Contributor III

Hello,

I'm writing a linux kernel driver in order to control the 6 IRQs on the P1020.

My approach is to configure those IRqs in the device tree, to map them using irq_of_parse_and_map, to request them using request_irq

and to get the ISRs using the Read system call and the waitqueue. so far so good.

But I would like to configure the registers in order to set the priorities. Is the best approach to directly (atomic) write the PIC_EIVPR0...PIC_EIVPR6 registers?

is there any freescale approach to set the interrupt priorities on the QorIQ with Linux?

Thanks a lot for your reply

ラベル(2)
1 解決策
3,785件の閲覧回数
scottwood
NXP Employee
NXP Employee

mpic_irq_set_priority()

Note that interrupts are disabled while running an interrupt handler, so this won't allow a high priority interrupt to preempt a low priority interrupt.  It will still ensure that the highest priority interrupt is the next one to be processed after the current interrupt finishes.

元の投稿で解決策を見る

2 返答(返信)
3,786件の閲覧回数
scottwood
NXP Employee
NXP Employee

mpic_irq_set_priority()

Note that interrupts are disabled while running an interrupt handler, so this won't allow a high priority interrupt to preempt a low priority interrupt.  It will still ensure that the highest priority interrupt is the next one to be processed after the current interrupt finishes.

3,784件の閲覧回数
tsybezoff
Contributor II

so how can i preempt a low priority interrupt??? i need it

0 件の賞賛
返信