Hi,
I'm trying to build the following yocto image, fsl-image-full but I got this error:
[shadow@orcas]$ bitbake fsl-image-full
WARNING: Host distribution "Unknown" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |###############################################################################################| ETA: 00:00:00
Loaded 2204 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.22.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Unknown"
TARGET_SYS = "powerpc-fsl-linux-gnuspe"
MACHINE = "p1020rdb"
DISTRO = "fsl-networking"
DISTRO_VERSION = "1.6"
TUNE_FEATURES = "m32 spe ppce500v2"
TARGET_FPU = "ppc-efd"
meta
meta-yocto
meta-yocto-bsp = "(detachedfromfsl-sdk-v1.6):0d2ce44c2b0f8cc9699e30cca2c24655be89d58b"
meta-fsl-ppc = "(detachedfromfsl-sdk-v1.6):6cf59d9de63a9fc5f8942c0d10c622898f4315ce"
meta-fsl-ppc-toolchain = "(detachedfromfsl-sdk-v1.6):a546e42f86e7d57de19e27907365d170b13fc18f"
meta-fsl-networking
meta-fsl-networking = "(detachedfrom8dec9c6):8dec9c690188cce5305ef5055f91e5cfa35c63f4"
meta-virtualization
meta-virtualization = "(detachedfromfsl-sdk-v1.6):8044073f63a0d99541a43ac5f2f6d789f94c7c7c"
meta-oe
meta-networking
meta-webserver
meta-ruby
meta-filesystems = "(detachedfromfsl-sdk-v1.6):b86007f742a1b829ccc8d76e485bb3f789cefaa4"
meta-java = "(detachedfromfsl-sdk-v1.6):d01f7d39e513790ddce20e6724723722119a3700"
meta-openstack
meta-openstack-compute-deploy
meta-openstack-controller-deploy
meta-openstack-qemu = "(detachedfromfsl-sdk-v1.6):f627404399a134672e0b5e26a0d9b794a6f8adf4"
NOTE: Preparing runqueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: Failed to fetch URL git://git.am.freescale.net/gitolite/sdk/hyperrelay.git, attempting MIRRORS if available
WARNING: Failed to fetch URL git://git.am.freescale.net/gitolite/libppc.git, attempting MIRRORS if available
ERROR: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/opt/fsl/yocto/build_p1020rdb_release/../sources/git2/git.am.freescale.net.gitolite.sdk.hyperrelay.git'...
2014/10/09 15:21:32 socat[29235] E CONNECT git.am.freescale.net:9418: Service Unavailable
fatal: Could not read from remote repository.
Please make sure you have the correct access rights
and the repository exists.
ERROR: Function failed: Fetcher failure for URL: 'git://git.am.freescale.net/gitolite/sdk/hyperrelay.git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /opt/fsl/build_p1020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/hyperrelay/git-r0/temp/log.do_fetch.29205
ERROR: Task 527 (/opt/fsl/meta-fsl-networking/recipes-extended/hyperrelay/hyperrelay_git.bb, do_fetch) failed with exit code '1'
ERROR: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/opt/fsl/yocto/build_p1020rdb_release/../sources/git2/git.am.freescale.net.gitolite.libppc.git'...
2014/10/09 15:21:32 socat[29232] E CONNECT git.am.freescale.net:9418: Service Unavailable
fatal: Could not read from remote repository.
Please make sure you have the correct access rights
and the repository exists.
ERROR: Function failed: Fetcher failure for URL: 'git://git.am.freescale.net/gitolite/libppc.git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /opt/fsl/build_p1020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/libppc/git-r0/temp/log.do_fetch.29203
ERROR: Task 751 (/opt/fsl/meta-fsl-networking/recipes-bsp/libppc/libppc_git.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 838 tasks of which 798 didn't need to be rerun and 2 failed.
Waiting for 0 running tasks to finish:
Summary: 2 tasks failed:
/opt/fsl/meta-fsl-networking/recipes-extended/hyperrelay/hyperrelay_git.bb, do_fetch
/opt/fsl/meta-fsl-networking/recipes-bsp/libppc/libppc_git.bb, do_fetch
Summary: There were 3 WARNING messages shown.
Summary: There were 4 ERROR messages shown, returning a non-zero exit code.
The source sdk iso does not contain the souces for these packages.
The only file it has in the sources directory are:
git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz
git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz.done
git2_git.am.freescale.net.gitolite.libppc.git.tar.gz
git2_git.am.freescale.net.gitolite.libppc.git.tar.gz.done
This is from the source sdk iso: QorIQ-SDK-V1.6-SOURCE-20140619-yocto.iso
Anyone know where I can get the source to libppc and hyperrelay?
I believe these are the only missing packages for a successful build.
Any help is appreciated.
Thanks,
- binh
已解决! 转到解答。
Hello Binh,
I am not sure where you modified local.conf file, did you modify source download dir in local.conf?
According to your description, it seems that you didn't use the formal installation procedure, I wrote an application note about how to use Yocto SDK, please refer to section 1 of QorIQ Linux SDK 1.6 Working With Yocto. Please note to install both "Source" and "Cache binary" ISOs, and use "install" script which will do necessary checking.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Binh,
The tar balls "git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz" and "git2_git.am.freescale.net.gitolite.libppc.git.tar.gz" are sources where Yocto bitbake build requires.
If the source tar ball md5sum is same with the value in the recipe, bitbake will not do "fetch" task, so your build environment works abnormally, did you do some modifications after install the ISO? For example, modify source tar ball or do cleanall command.
Please check md5 values of these two source tar balls in /opt/fsl/sources folder, whether they are same with the default.
5a297d3ed23e8c7f35ba355c4b9a309d sources/git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz
[b25805@sun QorIQ-SDK-V1.6-20140619-yocto]$ md5sum sources/git2_git.am.freescale.net.gitolite.libppc.git.tar.gz
bddb108e5f2c1bd61b1cee4b418a46a0 sources/git2_git.am.freescale.net.gitolite.libppc.git.tar.gz
In addition, it's better to install the Cache Binary ISO along with SOURCE ISO to avoid to build everything from the scratch.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
The md5sum matches:
[shadow@orcas]$ md5sum git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz
5a297d3ed23e8c7f35ba355c4b9a309d git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz
[shadow@orcas]$ md5sum git2_git.am.freescale.net.gitolite.libppc.git.tar.gz
bddb108e5f2c1bd61b1cee4b418a46a0 git2_git.am.freescale.net.gitolite.libppc.git.tar.gz
[shadow@orcas]$
I didn't make any changes except to local.conf. These were the steps I took:
- I untarred yocto.tar.gz
- source fsl-setup-poky -m p1020rdb
- modified local.conf
- bitbake fsl-image-full
Thanks,
- binh
Hello Binh,
I am not sure where you modified local.conf file, did you modify source download dir in local.conf?
According to your description, it seems that you didn't use the formal installation procedure, I wrote an application note about how to use Yocto SDK, please refer to section 1 of QorIQ Linux SDK 1.6 Working With Yocto. Please note to install both "Source" and "Cache binary" ISOs, and use "install" script which will do necessary checking.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
I added this to local.conf:
INHERIT += "rm_work"
In any case, I reinstalled using the install script and it built.
Now I have problems booting the image, it would kernel panic.
I'll start another post about that.
Thanks,
- binh