Error building p1020rdb yocto project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error building p1020rdb yocto project

Jump to solution
3,173 Views
binh
Contributor I

Hi,

I'm trying to build the following yocto image, fsl-image-full but I got this error:

[shadow@orcas]$ bitbake fsl-image-full

WARNING: Host distribution "Unknown" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.

Loading cache: 100% |###############################################################################################| ETA:  00:00:00

Loaded 2204 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Unknown"

TARGET_SYS        = "powerpc-fsl-linux-gnuspe"

MACHINE           = "p1020rdb"

DISTRO            = "fsl-networking"

DISTRO_VERSION    = "1.6"

TUNE_FEATURES     = "m32 spe ppce500v2"

TARGET_FPU        = "ppc-efd"

meta             

meta-yocto       

meta-yocto-bsp    = "(detachedfromfsl-sdk-v1.6):0d2ce44c2b0f8cc9699e30cca2c24655be89d58b"

meta-fsl-ppc      = "(detachedfromfsl-sdk-v1.6):6cf59d9de63a9fc5f8942c0d10c622898f4315ce"

meta-fsl-ppc-toolchain = "(detachedfromfsl-sdk-v1.6):a546e42f86e7d57de19e27907365d170b13fc18f"

meta-fsl-networking

meta-fsl-networking = "(detachedfrom8dec9c6):8dec9c690188cce5305ef5055f91e5cfa35c63f4"

meta-virtualization

meta-virtualization = "(detachedfromfsl-sdk-v1.6):8044073f63a0d99541a43ac5f2f6d789f94c7c7c"

meta-oe          

meta-networking  

meta-webserver   

meta-ruby        

meta-filesystems  = "(detachedfromfsl-sdk-v1.6):b86007f742a1b829ccc8d76e485bb3f789cefaa4"

meta-java         = "(detachedfromfsl-sdk-v1.6):d01f7d39e513790ddce20e6724723722119a3700"

meta-openstack   

meta-openstack-compute-deploy

meta-openstack-controller-deploy

meta-openstack-qemu = "(detachedfromfsl-sdk-v1.6):f627404399a134672e0b5e26a0d9b794a6f8adf4"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

WARNING: Failed to fetch URL git://git.am.freescale.net/gitolite/sdk/hyperrelay.git, attempting MIRRORS if available

WARNING: Failed to fetch URL git://git.am.freescale.net/gitolite/libppc.git, attempting MIRRORS if available

ERROR: Fetcher failure: Fetch command failed with exit code 128, output:

Cloning into bare repository '/opt/fsl/yocto/build_p1020rdb_release/../sources/git2/git.am.freescale.net.gitolite.sdk.hyperrelay.git'...

2014/10/09 15:21:32 socat[29235] E CONNECT git.am.freescale.net:9418: Service Unavailable

fatal: Could not read from remote repository.

Please make sure you have the correct access rights

and the repository exists.

ERROR: Function failed: Fetcher failure for URL: 'git://git.am.freescale.net/gitolite/sdk/hyperrelay.git'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /opt/fsl/build_p1020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/hyperrelay/git-r0/temp/log.do_fetch.29205

ERROR: Task 527 (/opt/fsl/meta-fsl-networking/recipes-extended/hyperrelay/hyperrelay_git.bb, do_fetch) failed with exit code '1'

ERROR: Fetcher failure: Fetch command failed with exit code 128, output:

Cloning into bare repository '/opt/fsl/yocto/build_p1020rdb_release/../sources/git2/git.am.freescale.net.gitolite.libppc.git'...

2014/10/09 15:21:32 socat[29232] E CONNECT git.am.freescale.net:9418: Service Unavailable

fatal: Could not read from remote repository.

Please make sure you have the correct access rights

and the repository exists.

ERROR: Function failed: Fetcher failure for URL: 'git://git.am.freescale.net/gitolite/libppc.git'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /opt/fsl/build_p1020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/libppc/git-r0/temp/log.do_fetch.29203

ERROR: Task 751 (/opt/fsl/meta-fsl-networking/recipes-bsp/libppc/libppc_git.bb, do_fetch) failed with exit code '1'

NOTE: Tasks Summary: Attempted 838 tasks of which 798 didn't need to be rerun and 2 failed.

Waiting for 0 running tasks to finish:

Summary: 2 tasks failed:

  /opt/fsl/meta-fsl-networking/recipes-extended/hyperrelay/hyperrelay_git.bb, do_fetch

  /opt/fsl/meta-fsl-networking/recipes-bsp/libppc/libppc_git.bb, do_fetch

Summary: There were 3 WARNING messages shown.

Summary: There were 4 ERROR messages shown, returning a non-zero exit code.

The source sdk iso does not contain the souces for these packages.

The only file it has in the sources directory are:

git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz

git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz.done

git2_git.am.freescale.net.gitolite.libppc.git.tar.gz

git2_git.am.freescale.net.gitolite.libppc.git.tar.gz.done

This is from the source sdk iso: QorIQ-SDK-V1.6-SOURCE-20140619-yocto.iso

Anyone know where I can get the source to libppc and hyperrelay?

I believe these are the only missing packages for a successful build.

Any help is appreciated.

Thanks,

- binh

Labels (1)
0 Kudos
Reply
1 Solution
1,888 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Binh,

I am not sure where you modified local.conf file, did you modify source download dir in local.conf?

According to your description, it seems that you didn't use the formal installation procedure, I wrote an application note about how to use Yocto SDK, please refer to section 1 of QorIQ Linux SDK 1.6 Working With Yocto. Please note to install both "Source" and "Cache binary" ISOs, and use "install" script which will do necessary checking.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,888 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Binh,

The tar balls "git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz" and "git2_git.am.freescale.net.gitolite.libppc.git.tar.gz" are sources where Yocto bitbake build requires.

If the source tar ball md5sum is same with the value in the recipe, bitbake will not do "fetch" task, so your build environment works abnormally, did you do some modifications after install the ISO? For example, modify source tar ball or do cleanall command.

Please check md5 values of these two source tar balls in /opt/fsl/sources folder, whether they are same with the default.

5a297d3ed23e8c7f35ba355c4b9a309d  sources/git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz

[b25805@sun QorIQ-SDK-V1.6-20140619-yocto]$ md5sum sources/git2_git.am.freescale.net.gitolite.libppc.git.tar.gz

bddb108e5f2c1bd61b1cee4b418a46a0  sources/git2_git.am.freescale.net.gitolite.libppc.git.tar.gz

In addition, it's better to install the Cache Binary ISO along with SOURCE ISO to avoid to build everything from the scratch.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,888 Views
binh
Contributor I

Hi,

The md5sum matches:

[shadow@orcas]$ md5sum git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz

5a297d3ed23e8c7f35ba355c4b9a309d  git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz

[shadow@orcas]$ md5sum git2_git.am.freescale.net.gitolite.libppc.git.tar.gz

bddb108e5f2c1bd61b1cee4b418a46a0  git2_git.am.freescale.net.gitolite.libppc.git.tar.gz

[shadow@orcas]$

I didn't make any changes except to local.conf. These were the steps I took:

- I untarred yocto.tar.gz

- source fsl-setup-poky -m p1020rdb

- modified local.conf

- bitbake fsl-image-full

Thanks,

- binh

0 Kudos
Reply
1,889 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Binh,

I am not sure where you modified local.conf file, did you modify source download dir in local.conf?

According to your description, it seems that you didn't use the formal installation procedure, I wrote an application note about how to use Yocto SDK, please refer to section 1 of QorIQ Linux SDK 1.6 Working With Yocto. Please note to install both "Source" and "Cache binary" ISOs, and use "install" script which will do necessary checking.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,888 Views
binh
Contributor I

Hi,

I added this to local.conf:

INHERIT += "rm_work"

In any case, I reinstalled using the install script and it built.

Now I have problems booting the image, it would kernel panic.

I'll start another post about that.

Thanks,

- binh

0 Kudos
Reply