Do the RGMII reference clock inputs, EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040 have to running at boot time or can they be enabled after boot?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do the RGMII reference clock inputs, EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040 have to running at boot time or can they be enabled after boot?

1,379件の閲覧回数
aduarte
Contributor I

Do the RGMII reference clock inputs,  EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040have to running at boot time or can they be enabled after boot? .  I need to know if those two clocks have to be running at power up or if they can be enabled after boot up.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,227件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

EC1_GTX_CLK125 and EC2_GTX_CLK125 on the P2040 can be enabled after boot.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信