Do the RGMII reference clock inputs, EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040 have to running at boot time or can they be enabled after boot?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Do the RGMII reference clock inputs, EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040 have to running at boot time or can they be enabled after boot?

1,381 次查看
aduarte
Contributor I

Do the RGMII reference clock inputs,  EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040have to running at boot time or can they be enabled after boot? .  I need to know if those two clocks have to be running at power up or if they can be enabled after boot up.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,229 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

EC1_GTX_CLK125 and EC2_GTX_CLK125 on the P2040 can be enabled after boot.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复