about S32K144 Diagnostic coverage data source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

about S32K144 Diagnostic coverage data source

跳至解决方案
1,831 次查看
loveMaker
Contributor I

dear NXP friend

        About M4_S32K144_SCST_Library_FaultCoverage_Estimation report,There's an entry in the table called "lookup",in the lookup sheet,Where the indpendent events and mutually-exclusive events data source comes from?

        for example:sheet lookup Column B, row 2:"0.05" ,Column D, row 2"0.0028"

0 项奖励
回复
1 解答
1,818 次查看
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

note that for SCST we provide Diagnostic Coverage which is estimated, not measured. In general, the input data for this table is a pessimistic estimation which was verified e.g. by engineering expert judgment or by fault injection on previous CST projects.

E.g. 0.05 is probability that fault will be detected by a single test vector.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,819 次查看
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

note that for SCST we provide Diagnostic Coverage which is estimated, not measured. In general, the input data for this table is a pessimistic estimation which was verified e.g. by engineering expert judgment or by fault injection on previous CST projects.

E.g. 0.05 is probability that fault will be detected by a single test vector.

0 项奖励
回复
1,812 次查看
loveMaker
Contributor I

I see. Thank you very much

0 项奖励
回复