about S32K144 Diagnostic coverage data source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about S32K144 Diagnostic coverage data source

ソリューションへジャンプ
1,823件の閲覧回数
loveMaker
Contributor I

dear NXP friend

        About M4_S32K144_SCST_Library_FaultCoverage_Estimation report,There's an entry in the table called "lookup",in the lookup sheet,Where the indpendent events and mutually-exclusive events data source comes from?

        for example:sheet lookup Column B, row 2:"0.05" ,Column D, row 2"0.0028"

0 件の賞賛
返信
1 解決策
1,810件の閲覧回数
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

note that for SCST we provide Diagnostic Coverage which is estimated, not measured. In general, the input data for this table is a pessimistic estimation which was verified e.g. by engineering expert judgment or by fault injection on previous CST projects.

E.g. 0.05 is probability that fault will be detected by a single test vector.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,811件の閲覧回数
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

note that for SCST we provide Diagnostic Coverage which is estimated, not measured. In general, the input data for this table is a pessimistic estimation which was verified e.g. by engineering expert judgment or by fault injection on previous CST projects.

E.g. 0.05 is probability that fault will be detected by a single test vector.

0 件の賞賛
返信
1,804件の閲覧回数
loveMaker
Contributor I

I see. Thank you very much

0 件の賞賛
返信