Yocto scarthgap build of linux-qoriq image failing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto scarthgap build of linux-qoriq image failing

Jump to solution
684 Views
bloggins666
Contributor I

The MACHINE variable is set to the 1024rdb-64b compiling with the powerpc freescale 64bit compiler within Yocto (scarthgap).

I'm trying to port an older implementation of a customer's yocto build environment from a dunfell based system to the scarthgap version.

As the system is building I've managed to fix a few issues but when it comes to building the linux-qoriq package the build fails. I've attached the log.

What is strange is that if I go into the devshell and build the same code using the customers defconfig file, it compiles without issue but the bitbake -c compile linux-qoriq definitely fails in the compile process.

Any advice as to how to break this down or fix it will be greatly appreciated.

 

Cheers!!

0 Kudos
Reply
1 Solution
547 Views
June_Lu
NXP TechSupport
NXP TechSupport

We have a distro release Dunfell which include the T1024. For the document of this release, You can take this for reference

https://docs.nxp.com/bundle/GUID-E5527A77-2F97-4244-BF9C-D08F068EFD16/page/GUID-2BDBF943-FBB7-46C3-8...

But we don't have continuous support on this release and NXP has no SDK upgrade plan on this product as well.

View solution in original post

0 Kudos
Reply
3 Replies
548 Views
June_Lu
NXP TechSupport
NXP TechSupport

We have a distro release Dunfell which include the T1024. For the document of this release, You can take this for reference

https://docs.nxp.com/bundle/GUID-E5527A77-2F97-4244-BF9C-D08F068EFD16/page/GUID-2BDBF943-FBB7-46C3-8...

But we don't have continuous support on this release and NXP has no SDK upgrade plan on this product as well.

0 Kudos
Reply
556 Views
bloggins666
Contributor I

T1024NXE7PQA

0 Kudos
Reply
621 Views
June_Lu
NXP TechSupport
NXP TechSupport

Please kindly share the part number of the MPU.

0 Kudos
Reply