The MACHINE variable is set to the 1024rdb-64b compiling with the powerpc freescale 64bit compiler within Yocto (scarthgap).
I'm trying to port an older implementation of a customer's yocto build environment from a dunfell based system to the scarthgap version.
As the system is building I've managed to fix a few issues but when it comes to building the linux-qoriq package the build fails. I've attached the log.
What is strange is that if I go into the devshell and build the same code using the customers defconfig file, it compiles without issue but the bitbake -c compile linux-qoriq definitely fails in the compile process.
Any advice as to how to break this down or fix it will be greatly appreciated.
Cheers!!
解決済! 解決策の投稿を見る。
We have a distro release Dunfell which include the T1024. For the document of this release, You can take this for reference
But we don't have continuous support on this release and NXP has no SDK upgrade plan on this product as well.
We have a distro release Dunfell which include the T1024. For the document of this release, You can take this for reference
But we don't have continuous support on this release and NXP has no SDK upgrade plan on this product as well.
T1024NXE7PQA
Please kindly share the part number of the MPU.