I am currently using the 1169 SBC and have encountered an issue while working with this chip. To trigger an over-voltage event, I continuously inject a 7V voltage into the VEXT pin. The software successfully detects the VEXTO event in the Supply Event Status Register.
However, after I clear the event by writing a 1 to the register, I can no longer detect the VEXTO event again. The event only appears again if I stop the fault injection and re-inject it. Why is this happening?
I was hoping to implement a debounce mechanism by continuously polling the VEXTO bit, but this approach doesn't seem to be feasible.Can you help me?
UJA1169TK
Dear Baikian,
please note, the UJA1169TK is End Of Life. The recommended replacement is UJA1169ATK. This is a normal behavior. If you clear the fault, it means the OV fault is not present anymore and you need to start the fault injection again.
With Best Regards,
Jozef