VR5510 Temperature calculation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VR5510 Temperature calculation

Jump to solution
3,011 Views
Girish1984
Contributor I

Hello,

I have a general question w.r.t temperature calculation from the data sheet of VR5510 Multi-Output PMIC.

Vtemp25 : Temperature Sensor Voltage at 25 deg C : Min 0.67V : Typ: 0.69V : Max : 0.71V

Vtemp_coeff : Temperature Sensor Coefficient : Min -2 : Typ --  : Max -1.9 mV/degC

Kindly let me know on how do I calculate temperature.

Thanks.

Tags (1)
0 Kudos
Reply
1 Solution
2,962 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Girish, 

a formula to calculate the temperature in the VR5510 temperature sensor is T(°C) = [(VAMUX – VTEMP25) /VTEMP_COEFF] + 25. It's for the typical value. I have created an excel file with a graph comparing the temperature with the measured voltage. Please find it attached.

With Best Regards,

Jozef 

View solution in original post

2 Replies
2,690 Views
sbobos
Contributor I

Hello @JozefKozon, 

I have one additional question about this topic. How we can get the VAMUX value in voltages? When we read the Amux channel for temperature we get value in digital representation, but in a formula, we are using voltage values.

Tags (2)
0 Kudos
Reply
2,963 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Girish, 

a formula to calculate the temperature in the VR5510 temperature sensor is T(°C) = [(VAMUX – VTEMP25) /VTEMP_COEFF] + 25. It's for the typical value. I have created an excel file with a graph comparing the temperature with the measured voltage. Please find it attached.

With Best Regards,

Jozef