VR5510 Temperature calculation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VR5510 Temperature calculation

ソリューションへジャンプ
3,010件の閲覧回数
Girish1984
Contributor I

Hello,

I have a general question w.r.t temperature calculation from the data sheet of VR5510 Multi-Output PMIC.

Vtemp25 : Temperature Sensor Voltage at 25 deg C : Min 0.67V : Typ: 0.69V : Max : 0.71V

Vtemp_coeff : Temperature Sensor Coefficient : Min -2 : Typ --  : Max -1.9 mV/degC

Kindly let me know on how do I calculate temperature.

Thanks.

タグ(1)
0 件の賞賛
返信
1 解決策
2,961件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Girish, 

a formula to calculate the temperature in the VR5510 temperature sensor is T(°C) = [(VAMUX – VTEMP25) /VTEMP_COEFF] + 25. It's for the typical value. I have created an excel file with a graph comparing the temperature with the measured voltage. Please find it attached.

With Best Regards,

Jozef 

元の投稿で解決策を見る

2 返答(返信)
2,689件の閲覧回数
sbobos
Contributor I

Hello @JozefKozon, 

I have one additional question about this topic. How we can get the VAMUX value in voltages? When we read the Amux channel for temperature we get value in digital representation, but in a formula, we are using voltage values.

タグ(2)
0 件の賞賛
返信
2,962件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Girish, 

a formula to calculate the temperature in the VR5510 temperature sensor is T(°C) = [(VAMUX – VTEMP25) /VTEMP_COEFF] + 25. It's for the typical value. I have created an excel file with a graph comparing the temperature with the measured voltage. Please find it attached.

With Best Regards,

Jozef