VR5510 Temperature calculation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

VR5510 Temperature calculation

跳至解决方案
3,021 次查看
Girish1984
Contributor I

Hello,

I have a general question w.r.t temperature calculation from the data sheet of VR5510 Multi-Output PMIC.

Vtemp25 : Temperature Sensor Voltage at 25 deg C : Min 0.67V : Typ: 0.69V : Max : 0.71V

Vtemp_coeff : Temperature Sensor Coefficient : Min -2 : Typ --  : Max -1.9 mV/degC

Kindly let me know on how do I calculate temperature.

Thanks.

标记 (1)
0 项奖励
回复
1 解答
2,972 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Girish, 

a formula to calculate the temperature in the VR5510 temperature sensor is T(°C) = [(VAMUX – VTEMP25) /VTEMP_COEFF] + 25. It's for the typical value. I have created an excel file with a graph comparing the temperature with the measured voltage. Please find it attached.

With Best Regards,

Jozef 

在原帖中查看解决方案

2 回复数
2,700 次查看
sbobos
Contributor I

Hello @JozefKozon, 

I have one additional question about this topic. How we can get the VAMUX value in voltages? When we read the Amux channel for temperature we get value in digital representation, but in a formula, we are using voltage values.

标记 (2)
0 项奖励
回复
2,973 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Girish, 

a formula to calculate the temperature in the VR5510 temperature sensor is T(°C) = [(VAMUX – VTEMP25) /VTEMP_COEFF] + 25. It's for the typical value. I have created an excel file with a graph comparing the temperature with the measured voltage. Please find it attached.

With Best Regards,

Jozef