USB Dongle preinstalled SW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Dongle preinstalled SW

ソリューションへジャンプ
2,077件の閲覧回数
aboi
Contributor I

Hi all,

 

I'd like to know if it is possible to load the 1322x USB Dongle preinstalled software to a 1322x network or sensor node. I'd like to use one of these nodes as sniffer. My problem is that I'm not able to find the code. Does anyone know if it is possible and where can I find the code? 

 

Thanks in advance,

aboi

0 件の賞賛
返信
1 解決策
1,683件の閲覧回数
tomlogic
Contributor III

Install WireShark and the WireShark ZigBee Utility.  You launch the utility from a command-prompt, passing in the COM port of the USB Dongle and the ZigBee channel you want to sniff.

 

Then you go into Wireshark and paste "\\.\pipe\wireshark" into the Interface field of teh Capture Options dialog.  Wireshark will then start displaying and decoding captured packets.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,684件の閲覧回数
tomlogic
Contributor III

Install WireShark and the WireShark ZigBee Utility.  You launch the utility from a command-prompt, passing in the COM port of the USB Dongle and the ZigBee channel you want to sniff.

 

Then you go into Wireshark and paste "\\.\pipe\wireshark" into the Interface field of teh Capture Options dialog.  Wireshark will then start displaying and decoding captured packets.

0 件の賞賛
返信