USB Dongle preinstalled SW

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB Dongle preinstalled SW

跳至解决方案
2,078 次查看
aboi
Contributor I

Hi all,

 

I'd like to know if it is possible to load the 1322x USB Dongle preinstalled software to a 1322x network or sensor node. I'd like to use one of these nodes as sniffer. My problem is that I'm not able to find the code. Does anyone know if it is possible and where can I find the code? 

 

Thanks in advance,

aboi

0 项奖励
回复
1 解答
1,684 次查看
tomlogic
Contributor III

Install WireShark and the WireShark ZigBee Utility.  You launch the utility from a command-prompt, passing in the COM port of the USB Dongle and the ZigBee channel you want to sniff.

 

Then you go into Wireshark and paste "\\.\pipe\wireshark" into the Interface field of teh Capture Options dialog.  Wireshark will then start displaying and decoding captured packets.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,685 次查看
tomlogic
Contributor III

Install WireShark and the WireShark ZigBee Utility.  You launch the utility from a command-prompt, passing in the COM port of the USB Dongle and the ZigBee channel you want to sniff.

 

Then you go into Wireshark and paste "\\.\pipe\wireshark" into the Interface field of teh Capture Options dialog.  Wireshark will then start displaying and decoding captured packets.

0 项奖励
回复