USB Dongle preinstalled SW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Dongle preinstalled SW

Jump to solution
2,124 Views
aboi
Contributor I

Hi all,

 

I'd like to know if it is possible to load the 1322x USB Dongle preinstalled software to a 1322x network or sensor node. I'd like to use one of these nodes as sniffer. My problem is that I'm not able to find the code. Does anyone know if it is possible and where can I find the code? 

 

Thanks in advance,

aboi

0 Kudos
Reply
1 Solution
1,730 Views
tomlogic
Contributor III

Install WireShark and the WireShark ZigBee Utility.  You launch the utility from a command-prompt, passing in the COM port of the USB Dongle and the ZigBee channel you want to sniff.

 

Then you go into Wireshark and paste "\\.\pipe\wireshark" into the Interface field of teh Capture Options dialog.  Wireshark will then start displaying and decoding captured packets.

View solution in original post

0 Kudos
Reply
1 Reply
1,731 Views
tomlogic
Contributor III

Install WireShark and the WireShark ZigBee Utility.  You launch the utility from a command-prompt, passing in the COM port of the USB Dongle and the ZigBee channel you want to sniff.

 

Then you go into Wireshark and paste "\\.\pipe\wireshark" into the Interface field of teh Capture Options dialog.  Wireshark will then start displaying and decoding captured packets.

0 Kudos
Reply