Tja1145 partial Network Wake up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tja1145 partial Network Wake up

Jump to solution
3,210 Views
1090097669
Contributor III

After configuring the partial network sleep process of the chip, after entering the Sleep Mode, when I uued the partial network wakes up the chip, it takes two frames to pull the RXD pin low, which wakes up the MCU. However, it is known from the OEM that only one frame can wake up the transceiver. And pull down the RXD pin, please inform the configuration of the error, thank you!

Labels (4)
0 Kudos
Reply
1 Solution
2,995 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this could be due to Autonomous bus biasing, as mentioned here https://community.nxp.com/message/890527

BR, Petr

View solution in original post

0 Kudos
Reply
1 Reply
2,996 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this could be due to Autonomous bus biasing, as mentioned here https://community.nxp.com/message/890527

BR, Petr

0 Kudos
Reply