Tja1145 partial Network Wake up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tja1145 partial Network Wake up

ソリューションへジャンプ
3,209件の閲覧回数
1090097669
Contributor III

After configuring the partial network sleep process of the chip, after entering the Sleep Mode, when I uued the partial network wakes up the chip, it takes two frames to pull the RXD pin low, which wakes up the MCU. However, it is known from the OEM that only one frame can wake up the transceiver. And pull down the RXD pin, please inform the configuration of the error, thank you!

ラベル(4)
0 件の賞賛
返信
1 解決策
2,994件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this could be due to Autonomous bus biasing, as mentioned here https://community.nxp.com/message/890527

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,995件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this could be due to Autonomous bus biasing, as mentioned here https://community.nxp.com/message/890527

BR, Petr

0 件の賞賛
返信