Tja1145 partial Network Wake up

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Tja1145 partial Network Wake up

跳至解决方案
3,207 次查看
1090097669
Contributor III

After configuring the partial network sleep process of the chip, after entering the Sleep Mode, when I uued the partial network wakes up the chip, it takes two frames to pull the RXD pin low, which wakes up the MCU. However, it is known from the OEM that only one frame can wake up the transceiver. And pull down the RXD pin, please inform the configuration of the error, thank you!

标签 (4)
0 项奖励
回复
1 解答
2,992 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this could be due to Autonomous bus biasing, as mentioned here https://community.nxp.com/message/890527

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,993 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this could be due to Autonomous bus biasing, as mentioned here https://community.nxp.com/message/890527

BR, Petr

0 项奖励
回复