TJA1153 pinnig

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TJA1153 pinnig

跳至解决方案
1,261 次查看
sametsan88
Contributor I

Hello


TJA1153 is same pinning with TJA1043. Right ? 
If it is not, how can i learn TJA1153 pins ? 

 

Thank you

0 项奖励
回复
1 解答
1,246 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Samet,

Yes, it is the same, except pins #8 (internally connected, should be left floating) and #11 (not connected). You can find the pin configuration in chapter 5 of the TJA1153A datasheet which is classified as a secure file requiring an NDA.

Capture.JPG

Capture 1.JPG

BR, Tomas

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,247 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Samet,

Yes, it is the same, except pins #8 (internally connected, should be left floating) and #11 (not connected). You can find the pin configuration in chapter 5 of the TJA1153A datasheet which is classified as a secure file requiring an NDA.

Capture.JPG

Capture 1.JPG

BR, Tomas

0 项奖励
回复