TJA1153 pinnig

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,258件の閲覧回数
sametsan88
Contributor I

Hello


TJA1153 is same pinning with TJA1043. Right ? 
If it is not, how can i learn TJA1153 pins ? 

 

Thank you

0 件の賞賛
返信
1 解決策
1,243件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Samet,

Yes, it is the same, except pins #8 (internally connected, should be left floating) and #11 (not connected). You can find the pin configuration in chapter 5 of the TJA1153A datasheet which is classified as a secure file requiring an NDA.

Capture.JPG

Capture 1.JPG

BR, Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,244件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Samet,

Yes, it is the same, except pins #8 (internally connected, should be left floating) and #11 (not connected). You can find the pin configuration in chapter 5 of the TJA1153A datasheet which is classified as a secure file requiring an NDA.

Capture.JPG

Capture 1.JPG

BR, Tomas

0 件の賞賛
返信