Hello
TJA1153 is same pinning with TJA1043. Right ?
If it is not, how can i learn TJA1153 pins ?
Thank you
Solved! Go to Solution.
Hello Samet,
Yes, it is the same, except pins #8 (internally connected, should be left floating) and #11 (not connected). You can find the pin configuration in chapter 5 of the TJA1153A datasheet which is classified as a secure file requiring an NDA.
BR, Tomas
Hello Samet,
Yes, it is the same, except pins #8 (internally connected, should be left floating) and #11 (not connected). You can find the pin configuration in chapter 5 of the TJA1153A datasheet which is classified as a secure file requiring an NDA.
BR, Tomas