SD8997 Wi-Fi Fails to Recover After In-Band Reset Triggered by EAPOL Timeout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SD8997 Wi-Fi Fails to Recover After In-Band Reset Triggered by EAPOL Timeout

1,494 次查看
yangyaoguang
Contributor III

Hi NXP Support Team,

I would like to report a new issue we encountered during our ongoing testing of the SD8997 Wi-Fi module in 5GHz STA mode.

Issue Description

Under repeated connection failure scenarios, particularly when multiple EAPOL timeouts occur (e.g., 5 consecutive failures), the driver triggers an in-band reset. However, we have observed that the firmware sometimes fails to reload afterward via the SDIO interface, leaving the Wi-Fi interface non-functional until the system is manually rebooted.

This behavior seems to occur only under reconnection stress conditions and may be related to how the SDIO interface or firmware handles recovery following a reset.

Platform Details

Driver Parameters

cfg80211_wext=0xf  
max_vir_bss=1  
cal_data_cfg=none  
ps_mode=2  
auto_ds=2  
host_mlme=1  
fw_name=nxp/sdiouart8997_combo_v4.bin  
drv_mode=3  
sta_name=wlan  
max_uap_bss=2  
txpwrlimit_cfg=nxp/tx_power_test.bin

Test Setup

  • Topology: SD8997 (STA) ←→ Access Point

  • Test Scenario: STA reconnection stress test

  • Failure Point: Firmware fails to reload after in-band reset, triggered by EAPOL timeouts

Relevant dmesg Logs:

[87697.429777] WiFi Reset due to EAPOL timeout cnt 5  
[87697.499968] ========START IN-BAND RESET===========  
[87704.130302] wlan_sdio_poll_card_status failed, tries = 10000, cs = 0xc  
[87704.259872] wlan_dnld_fw fail ret=0xffffffff  
[87705.481337] woal_request_fw failed  
[87705.484769] Firmware Init Failed

Request

We would greatly appreciate your help in confirming the following:

  • Is this a known issue with SDIO firmware reload after in-band reset?

  • Are there any suggested workarounds or firmware/driver updates available?

  • Would this require escalation to the SAE team for deeper investigation?

Please let us know if you need additional logs, debug configurations, or if any specific testing is required from our side. We’re happy to support further troubleshooting.

Thank you very much for your continued assistance.

Best regards,
Yaoguang

 

Attachment: dmesg.txt – captured during failure event for reference.

0 项奖励
回复
21 回复数

1,477 次查看
yangyaoguang
Contributor III

Attachment: dmesg.txt – captured during failure event for reference.

0 项奖励
回复

1,381 次查看
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yangyaoguang 

Just for your information, I have created an internal case to escalate this case.

Once have any updates, I will let you know.

 

Best regards,

Christine.

0 项奖励
回复

1,377 次查看
yangyaoguang
Contributor III

Hi Christine,

Noted, thank you!

Best regards,
Yaoguang

0 项奖励
回复

1,435 次查看
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yangyaoguang 

Thanks for creating new case to us.

I will check and reply to you ASAP.

For your information, this issue is related to FW reset, it might need our internal SAE team's help for tracking root cause. In other words, it will take longer time for global communications. Please pay more patient about this.

Thanks for your understandings!

 

Best regards,

Christine.

0 项奖励
回复

1,304 次查看
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yangyaoguang 

Can you please help to remove this driver load parameter: fw_name=nxp/sdiouart8997_combo_v4.bin

Also please  copy both (WLAN only and combo FW) in /lib/firmware/nxp path and provide observation.

 

Thanks,

Christine.

0 项奖励
回复

1,294 次查看
yangyaoguang
Contributor III

Hi Christine,

Just to update you on two points:

1. Driver Load Parameter

We are not directly passing fw_name=nxp/sdiouart8997_combo_v4.bin in the driver load command.
Instead, we use the following command with a config file:

modprobe moal mod_para=nxp/wifi_mod_para.conf


Both the combo and WLAN-only firmware files have already been placed under /lib/firmware/nxp/.

Directory contents:

README_MLAN
ed_mac_ctrl_V3_8997.conf
mlanutl
sd8997_bt_v4.bin
sd8997_wlan_v4.bin
sdiouart8997_combo_v4.bin
sdsd8997_combo_v4.bin
tx_power_test.bin
txpwrlimit_cfg_8997.conf
wifi_mod_para.conf

 

2. STA Link Failure After Long Uptime

A new issue was recently reported by our internal testing team.

In a long-term stability test (non-reconnection scenario), the STA interface failed to reconnect after 24 days of continuous operation and required a full reboot to recover.
During this time, the device was only sending a single ping to an external host approximately every 60 seconds.

Key log:

Block woal_cfg80211_del_key in abnormal driver stateThe related log is attached for your reference.

Best regards,
Yaoguang

0 项奖励
回复

1,287 次查看
yangyaoguang
Contributor III

Regarding the second point, this issue was observed during long-term testing with an older Wi-Fi firmware, and we are now updating to the latest version to rerun the same test.

0 项奖励
回复

1,248 次查看
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yangyaoguang 

Thanks for your updating.

1. Yes, I know you are using following command with a config file:

modprobe moal mod_para=nxp/wifi_mod_para.conf

 I mean please modify this config file: /lib/firmware/nxp/wifi_mod_para.conf, remove below parameter.

fw_name=nxp/sdiouart8997_combo_v4.bin

 Yes, from your given directory contents, I see both combo and Wi-Fi only FW are put there.

Please remove this parameter in /lib/firmware/nxp/wifi_mod_para.conf, then let me know your test results.

 

For point 2, please create a new case to us, so that we can track one issue with one case.  In this way, we will not be confused and also won't miss any issue.

 

Best regards,

Christine.

0 项奖励
回复

1,245 次查看
yangyaoguang
Contributor III

 

Hi Christine,

Thanks for your instructions.

  1. We removed the fw_name=nxp/sdiouart8997_combo_v4.bin parameter from /lib/firmware/nxp/wifi_mod_para.conf as requested. However, after doing so, the Wi-Fi driver failed to initialize successfully.

[ 31.329658] wlan: Loading MWLAN driver
[ 31.349418] wlan: Register to Bus Driver...
[ 31.353928] vendor=0x02DF device=0x9141 class=0 function=1
[ 31.365740] Attach moal handle ops, card interface type: 0x104
[ 31.371789] rps set to 0 from module param
[ 31.384957] SD8997: init module param from usr cfg
[ 31.393341] card_type: SD8997, config block: 0
[ 31.398090] cfg80211_wext=0xf
[ 31.401682] max_vir_bss=1
[ 31.404360] cal_data_cfg=none
[ 31.407714] ps_mode = 2
[ 31.410394] auto_ds = 2
[ 31.416131] host_mlme=enable
[ 31.420715] drv_mode = 3
[ 31.423957] sta_name=wlan
[ 31.427305] max_uap_bss = 2
[ 31.430680] txpwrlimit_cfg=nxp/tx_power_test.bin
[ 31.435583] Mode PSD file name: nxp/tx_power_test.bin
[ 31.435772] SDIO: sdio_blk_size=256 max_blk_count=65535 max_segs=128 max_seg_size=65535
[ 31.449893] rx_work=1 cpu_num=4
[ 31.453130] Enable moal_recv_amsdu_packet
[ 31.457238] Attach mlan adapter operations.card_type is 0x104.
[ 31.467379] wlan: Enable TX SG mode
[ 31.470961] wlan: mpa_tx.buf_size=65280
[ 31.474870] wlan: Enable RX SG mode
[ 31.541283] Request firmware: nxp/sduart8997_combo_v4.bin
[ 31.547021] wlan_sdio mmc1:0001:1: Direct firmware load for nxp/sduart8997_combo_v4.bin failed with error -2
[ 31.557949] wlan_sdio mmc1:0001:1: Falling back to sysfs fallback for: nxp/sduart8997_combo_v4.bin
[ 31.572463] WLAN: request_firmware() failed, error code = -11
[ 31.578407] woal_request_fw failed
[ 31.582174] Firmware Init Failed
[ 31.589377] Free module params
[ 31.592582] woal_add_card failed
[ 31.596264] wlan_sdio: probe of mmc1:0001:1 failed with error -1
[ 31.604477] usbcore: registered new interface driver usbxxx
[ 31.610456] wlan: Register to Bus Driver Done
[ 31.615067] wlan: Driver loaded successfully

 As a result, no interface appears under iw dev.

  1. Regarding the long-term STA issue: we will continue testing using the new firmware/driver version. If the issue can be reproduced again, we’ll proceed to open a separate case.

Best regards,
Yaoguang

0 项奖励
回复

1,237 次查看
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yangyaoguang 

Thanks for your quick response.

Sure, Let me check internally and reply you soon.

 

Best regards,

Christine.

0 项奖励
回复

1,212 次查看
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yangyaoguang 

Thank you for the driver load logs. From logs we can see below:

[ 31.541283] Request firmware: nxp/sduart8997_combo_v4.bin

 

Please copy the available combo FW as follows:

cd /lib/firmware/nxp/

cp sdiouart8997_combo_v4.bin sduart8997_combo_v4.bin

 

Please let us know if you still observe driver load failure after above steps.

 

Thanks,

Christine.

0 项奖励
回复

1,193 次查看
yangyaoguang
Contributor III

 

Hi Christine,

We followed your instruction and copied the firmware file:

cp /lib/firmware/nxp/sdiouart8997_combo_v4.bin /lib/firmware/nxp/sduart8997_combo_v4.bin

After that, the Wi-Fi driver loaded successfully, and the firmware initialized as expected.
Here is part of the log:

[ 31.293027] wlan: Register to Bus Driver...
[ 31.298597] vendor=0x02DF device=0x9141 class=0 function=1
[ 31.304248] Attach moal handle ops, card interface type: 0x104
[ 31.310149] rps set to 0 from module param
[ 31.316040] SD8997: init module param from usr cfg
[ 31.320942] card_type: SD8997, config block: 0
[ 31.325442] cfg80211_wext=0xf
[ 31.328413] max_vir_bss=1
[ 31.332138] cal_data_cfg=none
[ 31.335330] ps_mode = 2
[ 31.338024] auto_ds = 2
[ 31.340495] host_mlme=enable
[ 31.343678] drv_mode = 3
[ 31.346425] sta_name=wlan
[ 31.349052] max_uap_bss = 2
[ 31.352108] txpwrlimit_cfg=nxp/tx_power_test.bin
[ 31.357979] Mode PSD file name: nxp/tx_power_test.bin
[ 31.358168] SDIO: sdio_blk_size=256 max_blk_count=65535 max_segs=128 max_seg_size=65535
[ 31.371521] rx_work=1 cpu_num=4
[ 31.375600] Enable moal_recv_amsdu_packet
[ 31.379863] Attach mlan adapter operations.card_type is 0x104.
[ 31.386878] wlan: Enable TX SG mode
[ 31.390609] wlan: mpa_tx.buf_size=65280
[ 31.394633] wlan: Enable RX SG mode
[ 31.421308] Request firmware: nxp/sduart8997_combo_v4.bin
[ 32.226230] Wlan: FW download over, firmwarelen=635964 downloaded 626844
[ 32.839565] imx-dwmac 30bf0000.ethernet eth1: Link is Up - 100Mbps/Full - flow control rx/tx
[ 32.945532] WLAN FW is active
[ 32.948508] on_time is 32943367625
[ 32.951962] Download txpwrlimit_cfg=nxp/tx_power_test.bin
[ 33.015199] VDLL image: len=9120
[ 33.098103] fw_cap_info=0x587c6fa3, dev_cap_mask=0xffffffff
[ 33.103931] max_p2p_conn = 8, max_sta_conn = 8
[ 33.111331] FW country code WW does not match with US
[ 33.142173] Register NXP 802.11 Adapter wlan0
[ 33.147973] wlan: uap%d set max_mtu 2000
[ 33.160450] Register NXP 802.11 Adapter uap0
[ 33.167250] wlan: uap%d set max_mtu 2000
[ 33.189411] Register NXP 802.11 Adapter uap1
[ 33.195525] wlan: version = SD8997----16.92.21.p149.2-MM6X16537.p9-GPL-(FP92)
[ 33.209366] usbcore: registered new interface driver usbxxx
[ 33.217078] wlan: Register to Bus Driver Done
[ 33.221474] wlan: Driver loaded successfully
[ 33.691546] wlan: wlan0 START SCAN

Best regards,
Yaoguang

0 项奖励
回复

1,187 次查看
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yangyaoguang 

Thanks for your quick reply.

Sounds great!

Then please help to check the original issue(Wi-Fi fails to recover after in-band reset triggered by EAPOL Timeout) whether still exist.

 

Best regards,

Christine.

0 项奖励
回复

993 次查看
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yangyaoguang 

Do you have any updates on this case?

Whether the original issue(Wi-Fi Fails to Recover After In-Band Reset Triggered by EAPOL Timeout) is still exist?

 

Best regards,

Christine.

0 项奖励
回复

990 次查看
yangyaoguang
Contributor III

Hi Christine,

This issue is still reproducible on our side. We may need some additional time to investigate it further, and we will provide feedback once we have any new findings.

Best regards,
Yangyaoguang

0 项奖励
回复

986 次查看
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yangyaoguang 

Thanks for your feedback.

If it still exist, would you please help to provide us dmesg logs for further tracking?

Hope we can resolve it ASAP.

Best regards,

Christine.

0 项奖励
回复

969 次查看
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yangyaoguang 

Can you please help get below logs and details?

  • dmesg logs (drvdbg=0xa0037)
  • Valid FW dumps when issue is observed.
  • The issue scenario and steps for better understanding and issue re-creation.

Best regards,

Christine.

0 项奖励
回复

894 次查看
yangyaoguang
Contributor III

Hi Christine,

It seems that the issue has been resolved. Based on the latest internal testing, the automation has been running for 4 days without encountering any issues. Previously, we could reproduce the problem within 1-3 hours, but with the changes we made (SDIO frequency set to 50MHz and the latest WIFI driver update), the issue no longer occurs.

Thank you for your support !

Best regards,
Yangyaoguang

标记 (1)
0 项奖励
回复

887 次查看
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yangyaoguang 

Thanks for your feedback.

Then would you please help to accept my answer as a solution so that we can close this current case?

For the SDIO frequency, let's continue to discuss in another thread, OK?

https://community.nxp.com/t5/Other-NXP-Products/URGENT-SD8997-WiFi-Module-5GHz-STA-Throughput-Freque...

 

Best regards,

Christine.

0 项奖励
回复

850 次查看
yangyaoguang
Contributor III

Hi Christine,

After our internal discussion, we also believe that this issue can be closed.

Best regards,
Yangyaoguang

标记 (1)
0 项奖励
回复