SC18IM704PWJ GPIO6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC18IM704PWJ GPIO6

Jump to solution
2,553 Views
jj100126
Contributor I

The datasheet says the following: 

gpio6.PNG

 

So does that mean that when making a design that uses the SC18, the GPIO6 must have a pull-up resistor to it?

0 Kudos
Reply
1 Solution
2,542 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Joshua,

Yes, the GPIO6 must have a pull-up resistor to ensure proper boot.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
3 Replies
2,379 Views
egershon
Contributor I

I am trying to connect the bridge to a half duplex UART (one wire arrangement),

I was thinking to activate through one of the I/O a one shot signal to control an external tri-state output buffer of the TX to enable Tx only when master on the UART expecting returned message. i was not sure if it can be done with the help of I2C on/off command

0 Kudos
Reply
2,543 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Joshua,

Yes, the GPIO6 must have a pull-up resistor to ensure proper boot.

Best regards,

Tomas

0 Kudos
Reply
2,489 Views
jj100126
Contributor I

Hello,

I'd like to know why the SC18 in the evaluation board boots up even though there's no pull-up resistor on its GPIO6? serial interface.PNG

0 Kudos
Reply