SC18IM704PWJ GPIO6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,549件の閲覧回数
jj100126
Contributor I

The datasheet says the following: 

gpio6.PNG

 

So does that mean that when making a design that uses the SC18, the GPIO6 must have a pull-up resistor to it?

0 件の賞賛
返信
1 解決策
2,538件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Joshua,

Yes, the GPIO6 must have a pull-up resistor to ensure proper boot.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,375件の閲覧回数
egershon
Contributor I

I am trying to connect the bridge to a half duplex UART (one wire arrangement),

I was thinking to activate through one of the I/O a one shot signal to control an external tri-state output buffer of the TX to enable Tx only when master on the UART expecting returned message. i was not sure if it can be done with the help of I2C on/off command

0 件の賞賛
返信
2,539件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Joshua,

Yes, the GPIO6 must have a pull-up resistor to ensure proper boot.

Best regards,

Tomas

0 件の賞賛
返信
2,485件の閲覧回数
jj100126
Contributor I

Hello,

I'd like to know why the SC18 in the evaluation board boots up even though there's no pull-up resistor on its GPIO6? serial interface.PNG

0 件の賞賛
返信