P1014 QorIQ Integrated Processors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1014 QorIQ Integrated Processors

1,036件の閲覧回数
PTusername
Contributor I

In case of P1014 QorIQ Integrated Processors

Link-  https://rocelec.widen.net/view/pdf/vr2ddso1wa/FSCLS11835-1.pdf?t.download=true&u=5oefqw

Please refer to Page 98, Table 86 last column in above link. .Are the die revs backward compatible?  Your help is highly appreciated.

E.g. Is P1014NXN5HHB  backward compatible to  P1014NXN5HHA?

 

 

 

 

0 件の賞賛
返信
1 返信

1,019件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The errata document for the p1010 which covers the p1014 as well. If you have this document, you can go through table 3 to identify which errata applies for Rev 1.0 "A" and Rev 2.01 "B" silicon of the P1014. Depending on the your use case and features that are enabled on the P1014, it may or may not be backward compatible.

0 件の賞賛
返信